AXIS#.MOTOR.TEMP
Description
This parameter returns the motor temperature, which is represented as the resistance of the motor's PTC or NTC.
Context
For more information see Motor and Motor Temperature View.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Ω |
Range |
0 to 232 Ω |
Default Value |
N/A |
Data Type |
Integer |
See Also |
N/A |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.MOTOR.TEMP | 0x500B | 0x2 | UDINT | - | - | RO | True |
AXIS2.MOTOR.TEMP | 0x510B | 0x2 | UDINT | - | - | RO | True |